Zoeken

Hoofdinhoud

  • Home
  • Poka Yoke – the accurate manual workstation
  • Registreren
  • Login

Factory Automation

Print page

Factory Automation

Poka Yoke – the accurate manual workstation

Despite digitalization and full automation, there are still complex activities that can only be processed manually. The zero-defect manual workstation offers a unique, cost-efficient and high-quality overall concept precisely for these requirements.

For your error-free manual work

The Japanese "Poka Yoke" approach means the systematic exclusion of human error through technical precautions.

Mitsubishi Electric and the assembly technology specialist HANDKE Industrietechnik have implemented a concept that offers you an efficient, modular and flexible zero-defect workstation.

When everything fits together perfectly

Whether assembly, order picking or logistics – even for applications with lot sizes 1 you are on the right track with this error-free manual workstation. It is equipped with profiles from the most common manufacturers and can be ergonomically adapted. In addition to a classic pick-by light system the system also has physical barriers in the form of door flaps.

The system is also interesting for the topic of human-machine/collaborative robotics – especially if, for example, pre-assembly is necessary or parts have to be handed over. This individually configurable and expandable concept was developed in the automotive industry and can be found in all branches of industry today.

Translated with www.DeepL.com/Translator

Your advantages at a glance

  • An intelligent workstation tailored to your individual needs
  • Variety of sensor technologies. From light barriers over Pick To Light pushbuttons to door flaps as a physical barrier. Zero-defect-quality guaranteed!
  • Simple start-up/setup of assembly- and commissioning sequences
  • Expandable system: fast implementation of electrical srewdrivers and barcode scanners
  • Optional connection with DB-services, to have access to production data anytime and anywhere in times of I4.0.
  • Door flaps as unique selling feature
  • Manage up to 128 sensors per shelf or 64 door flaps with the Poka Yoke Basic-Controller

Information flyer

The highlights of the Poka Yoke-Solution by Handke and Mitsubishi Electric briefly summarised are offered for download here.

The 2-sided info flyer ist available for download here

General information around Poka Yoke are offered for download here

The Poka Yoke-flyer is available for download here

Videos

Poka Yoke – the accurate manual workstation

Here, you can see how easy it is to integrate barcode scanners into the Poka Yoka-System

Fair video about the simple integration of barcode scanners

Poka Yoke – the accurate manual workstation

Here, you can see how fast, safe and error-free work can be done in only a few single steps

Fair video about Poka Yoke – easy and error-free

Poka Yoke – the accurate manual workstation

Here, you can see how sensitive and fast the sensor technology reacts at the manual workstation

Demonstration of the sensitivity of the sensor technology

Poka Yoke – the accurate manual workstation

Here, you can see how quick and simple the back can be filled

Quick and easy filling of the back

Poka Yoke on Twitter

https://twitter.com/handkeindustrie

https://twitter.com/MitsubishiFAEU


Did we arouse your interest? We would be pleased to present our Poka Yoke-solution to you personally. Just fill in the contact form and we will get in touch with you.

De met een * gemarkeerde velden moeten worden ingevuld.

Voer de tekst links op het scherm in het onderstaande veld in. Als u het scherm niet kunt lezen, klik dan op "Bijwerken".

Sicherheitscode Bijwerken

terug

Omhoog